hanging at start up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

hanging at start up

3,284 Views
Frost
Contributor II

I have codewarrior 10.4 / Win7 x64. (eval)

 

Every time I start it up, it hangs for ~50 seconds before the UI becomes available. It starts to load up, and says loading PE components, gets to 85% and hangs for nearly a minute.

 

This is a bit annoying. I'm running an i7 3930K @ 3.2GHz, 32GB of ram, and SSDs in raid 0. Is it waiting for updates? Can i set something to fix this? Is it a known bug?

 

Thanks

Labels (1)
0 Kudos
Reply
3 Replies

2,096 Views
bowerymarc
Contributor V

this just started happening to me with CW 10.5 with only 3 projects in my workspace.  Hanging trying to start PE, or InitRemoteEditJob, it's not clear.

But this thread: java - Eclipse will not start and I haven't changed anything - Stack Overflow

Led me to run this command which resets your window settings but everything else is intact and the hanging stops:

"C:\Freescale\CW MCU v10.5\eclipse\cwide.exe" -clean -clearPersistedState

good luck

0 Kudos
Reply

2,096 Views
Monica
Senior Contributor III

Hello Frost,

did this suggestions help you through the issue? Please keep us posted!

Best regards,

Monica.

0 Kudos
Reply

2,096 Views
BlackNight
NXP Employee
NXP Employee

No, that's not normal. I have a 2.2 GHz, i6, 4 GB RAM and normal harddisk, and it only takes less than 10 seconds.

It took longer (about one minute) the first time after installation to load PE components, but not afterwards.

Does it happen with a new/empty workspace too?

I know that if a workspace has > 50 projects, it takes somewhat longer (say around 15 seconds), but not in your ballpark.

Have you CodeWarrior installed in c:\Freescale? With full access rights to the folder?

Otherwise it could be the Processor Expert always re-scans the components. That would not be ok.

I hope this helps.

0 Kudos
Reply