for mcu .S19 file download

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

for mcu .S19 file download

跳至解决方案
3,605 次查看
lijiandong
Contributor I
how to download .s19 to 908 mcu chip?
I find the codewarrior for hc08  can't do that.
 
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,548 次查看
Alban
Senior Contributor II

Hi,

CodeWarrior for HC08 can do this. You need to have the proper interface in hardware as described in the datasheet of your product at the development support chapter.

Then, when your hardware is OK, you just need to select a basic Class I interface to program the MCU.

Also, you can use 3rd party tools, like a Cyclone or MON08 cable (there are many) that will handle more things automatically. Because if you use the basic interface, you need to power on/off/on the MCU during the programming sequence.

Cheers,
Alban.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,549 次查看
Alban
Senior Contributor II

Hi,

CodeWarrior for HC08 can do this. You need to have the proper interface in hardware as described in the datasheet of your product at the development support chapter.

Then, when your hardware is OK, you just need to select a basic Class I interface to program the MCU.

Also, you can use 3rd party tools, like a Cyclone or MON08 cable (there are many) that will handle more things automatically. Because if you use the basic interface, you need to power on/off/on the MCU during the programming sequence.

Cheers,
Alban.

0 项奖励
回复
1,548 次查看
peg
Senior Contributor IV

Hi,

To exactly what device and through which interface?

BR Peg

 

0 项奖励
回复