failed writing target address0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

failed writing target address0

1,400 次查看
barbercolman
Contributor III

  Derek

We a brand new k20 PCB and are attempting to program with a P&E Multilink U. Programming the part failed with a "failed writing target address0" a hardware issue or a problem with the new BSP/PSP we set up.

3743_3743.bmpScreenShot108.bmp

标签 (1)
标记 (4)
0 项奖励
回复
3 回复数

1,140 次查看
FarhanH
Contributor III

I have the same exact issue with a K60 PCB and Multilink U. We have two custom boards that are duplicates and one of them has this issue. I am wondering whether it has something to do with the chip memory, as in, it has accidentally been locked.

0 项奖励
回复

1,140 次查看
barbercolman
Contributor III

Actually in this case I found that there was problems in how we built the BSP as well as issues in the debugger setup.  I do not remember the final solution, but the primary cause was operator error!.

0 项奖励
回复

1,140 次查看
FarhanH
Contributor III

Yeah, I wouldn't be surprised. I think I have to go back and revisit the custom BSP debugger files to make sure it is flashing correctly.

0 项奖励
回复