failed writing target address0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

failed writing target address0

1,352件の閲覧回数
barbercolman
Contributor III

  Derek

We a brand new k20 PCB and are attempting to program with a P&E Multilink U. Programming the part failed with a "failed writing target address0" a hardware issue or a problem with the new BSP/PSP we set up.

3743_3743.bmpScreenShot108.bmp

ラベル(1)
タグ(4)
0 件の賞賛
返信
3 返答(返信)

1,092件の閲覧回数
FarhanH
Contributor III

I have the same exact issue with a K60 PCB and Multilink U. We have two custom boards that are duplicates and one of them has this issue. I am wondering whether it has something to do with the chip memory, as in, it has accidentally been locked.

0 件の賞賛
返信

1,092件の閲覧回数
barbercolman
Contributor III

Actually in this case I found that there was problems in how we built the BSP as well as issues in the debugger setup.  I do not remember the final solution, but the primary cause was operator error!.

0 件の賞賛
返信

1,092件の閲覧回数
FarhanH
Contributor III

Yeah, I wouldn't be surprised. I think I have to go back and revisit the custom BSP debugger files to make sure it is flashing correctly.

0 件の賞賛
返信