don't run without SWD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

don't run without SWD

976 次查看
PO220
Contributor IV

Hello

 

I just finished my firt application with MQX lite (and first application with Processor expert) for a KL15.

program works fine but when I turn on card supply without SWD, nothing happens ! LED life is not flashing, the various tasks do not work ...

How is this possible ? what should I do ?  activate in PE ?

 

thank you in advance

 

PS : My SWD is a multilink universal (green one)

标签 (1)
0 项奖励
回复
1 回复

798 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

please check these two possible reasons:

1. made sure your code is download in Flash but not RAM.

pastedImage_0.png

2. make sure you do not have selected any of the "XXX_hosted" options.

Re: MK10DX256VLK7 doesn't run standalone, just when debugging. Verified it's running from FLASH, not...

can this help you?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复