document for porting project from codewarrior v6.3 to codewarrior 10.4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

document for porting project from codewarrior v6.3 to codewarrior 10.4

Jump to solution
1,318 Views
hotashu
Contributor III

hi guys,

we have a project made under Codewarrior 6.3 before. now we want port it to 10.4. does Freescale have document for how to do it step by step?

Labels (1)
0 Kudos
Reply
1 Solution
952 Views
BlackNight
NXP Employee
NXP Employee

Hello,

such a document would heavily depend on your 6.3 document I think. Basically what I did is the following:

- create a new project with File > New > Bareboard project

- verify that it works with my board

- then add the sources from the 6.3 project, preferably step by step

There is a 'getting started' in 10.4 which describes the steps to create a project and then debug it, so this could be a starting point for you.

In MCU10.2 there was an 'importer' which imported 6.x projects. But such an importer only can work for very simply cases and projects, so you are faster and better with the steps above.

Some points to consider:

- compiler options: unless you need special things, go with the defaults in the first step, and then change them later on.

  You find the compiler options under (select the project) the menu Project > Properties > C/C++ Build > Settings

- include folders: depending on how you have organized your sources, you need to add the paths to the compiler search paths. The paths are set up in the compiler panels/settings under the menu in previous point.

Hope this helps.

View solution in original post

0 Kudos
Reply
2 Replies
952 Views
Monica
Senior Contributor III

Hello Hotas!

Did that help? Please keep us posted, we'd like to know :smileywink:

Best regards,

Monica.

0 Kudos
Reply
953 Views
BlackNight
NXP Employee
NXP Employee

Hello,

such a document would heavily depend on your 6.3 document I think. Basically what I did is the following:

- create a new project with File > New > Bareboard project

- verify that it works with my board

- then add the sources from the 6.3 project, preferably step by step

There is a 'getting started' in 10.4 which describes the steps to create a project and then debug it, so this could be a starting point for you.

In MCU10.2 there was an 'importer' which imported 6.x projects. But such an importer only can work for very simply cases and projects, so you are faster and better with the steps above.

Some points to consider:

- compiler options: unless you need special things, go with the defaults in the first step, and then change them later on.

  You find the compiler options under (select the project) the menu Project > Properties > C/C++ Build > Settings

- include folders: depending on how you have organized your sources, you need to add the paths to the compiler search paths. The paths are set up in the compiler panels/settings under the menu in previous point.

Hope this helps.

0 Kudos
Reply