cw v10.1 compiler patch install issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

cw v10.1 compiler patch install issue

7,531 Views
mikeu
Contributor I

I am attemting to install the 10.1 compiler update and get the following error:

Software being installed: MCU v10.1 Compiler Update (ColdFire, Kinetis) 1.0.0 (com.freescale.mcu10_1.buildtools.win.sp.feature.group 1.0.0)
  Missing requirement: MCU v10.1 Compiler Update (ColdFire, Kinetis) 1.0.0 (com.freescale.mcu10_1.buildtools.win.sp.feature.group 1.0.0) requires 'org.eclipse.ui.net [1.0.0.FSL_b15_2105-A21]' but it could not be found

 

I have edited the freescale location to add the trailing / as describes in the pdf for updating cw10.1

 

Here are my locations:

Freescale    http://freescale.com/lgfiles/updates/Eclipse/MCU10_1/com.freescale.mcu.updatesite/    EnabledFSL MCU Eclipse Update Site    http://freescale.com/lgfiles/updates/Eclipse/MCU/com.freescale.mcu.updatesite/    Enabled
update site: http://download.eclipse.org/dsdp/dd/updates    http://download.eclipse.org/dsdp/dd/updates    Enabled
update site: http://download.eclipse.org/tools/cdt/releases/ganymede    http://download.eclipse.org/tools/cdt/releases/ganymede    Enabled

Any thoughts as to why this does not work?

 

Thanks

Labels (1)
0 Kudos
Reply
10 Replies

6,116 Views
J2MEJediMaster
Specialist I

I understand that by installing a patch you are doing through the Eclipse update mechanism? Or did you download an installer?

 

---Tom

 

0 Kudos
Reply

6,116 Views
mikeu
Contributor I

I am attempting to apply the patch from Help -> Install new Software in Eclipse.

 

0 Kudos
Reply

6,116 Views
Kafre
Contributor III

Same trouble here.

 

I'm currently downloading the program again to make a clean reinstallation.

 

Note aside: Seems that some part of FSL SW is missing.

0 Kudos
Reply

6,116 Views
mikeu
Contributor I

All

 

I uninstalled 10.1 completely and did a clean install then modified the update url to add the trailing / as indicated by the cw10.1 update procedure pdf and it now works as it should.

 

Strange because I am not sure what was different than the first time.

0 Kudos
Reply

6,116 Views
juanee
Contributor III

It looks like the Codewarrior 10.1 compiler update is to update an existing Codewarrior 10.1 install.

 

Since I had Codewarrior 10.0 installed, that looks like the reason I couldn't install the update.

 

I installed CW 10.1 Special Edition (CW_MCU_v10.1_SE.exe) and was able to update that install as described in CW_MCU_v10.1_Update_Procedure.pdf.

 

I was also able to install MQX 3.7 after that.

 

Thanks everyone.

 

Juan

0 Kudos
Reply

6,116 Views
Kafre
Contributor III

Complete reinstallation solved the problem. 

0 Kudos
Reply

6,116 Views
J2MEJediMaster
Specialist I

I know that this is late, but it took me a while to track this down. For CodeWarrior v10 updates, you do NOT use Eclipse's Install Software option. You download the new CW version from the Freeescale website, and run the downloaded installer application. The CodeWarrior installer has a complete implementation of CodeWarrior, along with any updated tools or modules.

 

---Tom

0 Kudos
Reply

6,116 Views
LenZhao
Contributor I

I use help->Install new software and this website FSL MCU Eclipse Update Site - http://freescale.com/lgfiles/updates/Eclipse/MCU10_1/com.freescale.mcu.updatesite to update CW10.1, but the respond is below:

An error occurred while collecting items to be installed  session context was:smileysad:profile=PlatformProfile, phase=org.eclipse.equinox.internal.provisional.p2.engine.phases.Collect, operand=, action=).  No repository found containing: org.eclipse.update.feature,com.freescale.coretech.debugger.kasample,7.15.0.FSL_b8910  No repository found containing: binary,com.freescale.coretech.debugger.kasample_root,7.15.0.FSL_b8910  No repository found containing: osgi.bundle,com.freescale.debugger.kernel.aware.sample,7.15.0.FSL_b8910  No repository found containing: osgi.bundle,com.freescale.debugger.kernel.aware.sample.corba,7.15.0.FSL_b8910  No repository found containing: org.eclipse.update.feature,com.freescale.mcu.coldfiredb,1.0.1  No repository found containing: binary,com.freescale.mcu.coldfiredb_root,1.0.1  No repository found containing: org.eclipse.update.feature,com.freescale.mcu.mc13233.win.sp,1.0.2  No repository found containing: binary,com.freescale.mcu.mc13233.win.sp_root,1.0.2  No repository found containing: org.eclipse.update.feature,com.freescale.mcu10_1.buildtools.win.sp,1.0.0  No repository found containing: binary,com.freescale.mcu10_1.buildtools.win.sp_root,1.0.0  No repository found containing: org.eclipse.update.feature,com.freescale.mcu10_1.mcf51jf128.win.sp,1.0.3  No repository found containing: binary,com.freescale.mcu10_1.mcf51jf128.win.sp_root,1.0.3  No repository found containing: osgi.bundle,com.freescale.coldfire.cdt.gcc.toolchain,1.0.2.FSL_b02057  No repository found containing: osgi.bundle,com.freescale.coldfire.cdt.gcc.toolchain.nl1,1.0.2.FSL_b02057  No repository found containing: osgi.bundle,com.freescale.coldfire.cdt.toolchain,1.0.15.FSL_b02057  No repository found containing: osgi.bundle,com.freescale.coldfire.cdt.toolchain.nl1,1.0.15.FSL_b02057  No repository found containing: osgi.bundle,com.freescale.hc08.cdt.toolchain,1.0.17.FSL_b02057  No repository found containing: osgi.bundle,com.freescale.hc08.cdt.toolchain.nl1,1.0.17.FSL_b02057  No repository found containing: osgi.bundle,com.freescale.mcu,1.0.4.FSL_b02057  No repository found containing: osgi.bundle,com.freescale.mcu.cdt.toolchain,1.0.1.FSL_b02057  No repository found containing: osgi.bundle,com.freescale.mcu.changewizard,1.0.44.FSL_b02057  No repository found containing: osgi.bundle,com.freescale.mcu.changewizard.nl1,1.0.44.FSL_b02057  No repository found containing: osgi.bundle,com.freescale.mcu.elfimporter,10.1.5.FSL_b02057  No repository found containing: osgi.bundle,com.freescale.mcu.elfimporter.nl1,10.1.5.FSL_b02057  No repository found containing: osgi.bundle,com.freescale.mcu.license,10.1.0.FSL_b02057  No repository found containing: osgi.bundle,com.freescale.mcu.license.nl1,10.1.0.FSL_b02057  No repository found containing: osgi.bundle,com.freescale.mcu.linuxapp.projectwizard,1.1.8.FSL_b02057  No repository found containing: osgi.bundle,com.freescale.mcu.linuxapp.projectwizard.nl1,1.1.8.FSL_b02057  No repository found containing: osgi.bundle,com.freescale.mcu.nl1,1.0.4.FSL_b02057  No repository found containing: osgi.bundle,com.freescale.mcu.pathmapping,1.0.5.FSL_b02057  No repository found containing: osgi.bundle,com.freescale.mcu.projectWizard.nl1,1.3.46.FSL_b02057  No repository found containing: osgi.bundle,com.freescale.mcu.projectimporter,1.1.5.FSL_b02057  No repository found containing: osgi.bundle,com.freescale.mcu.projectimporter.nl1,1.1.5.FSL_b02057  No repository found containing: osgi.bundle,com.freescale.mcu.projectwizard,1.3.46.FSL_b02057  No repository found containing: osgi.bundle,com.freescale.mcu.ui,1.0.0.FSL_b02057  No repository found containing: org.eclipse.update.feature,com.freescale.mcu,10.1.3

 

How to deal with this problem?

Thanks.

0 Kudos
Reply

6,116 Views
KenH
Contributor II

I had the same problem. I made the problem go away by first completely uninstalling codewarrior, then nothing. We are not going to use this any more. Software should not be this much trouble to use. Good luck.

 

0 Kudos
Reply

6,116 Views
juanee
Contributor III

I have the same error trying to update codewarrior via the HELP->Install New Software... menu.

 

I tried both methods described in: CW_MCU_v10.1_Update_Procedure.pdf

 

Anyone know how to fix this?  Replies are appreciated.

 

Juan

 

Codewarrior 10 Special Edition

Windows XP Pro

MQX 3.6.2

PEMicro USB ColdFire Multilink.

Custom Target based on Coldfire MCF52259.

0 Kudos
Reply