create/add some sub-folders in my source folder

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

create/add some sub-folders in my source folder

1,507件の閲覧回数
amleng
Contributor IV

Hello Community,

 

How can I create/add some sub-folders in the Source Folder once I create a new MQX project?

These sub-folders can contain some other source files which could be located in other locations rather than ‘source’ folder.

A good example would be web_hvac project in atheros_wifi package. As you can see in the figure in Source folder

there are some other folders like ‘enet’ or ‘phy’. The actual location of these folders are somewhere else rather than

in the ‘source’ folder in the hard drive; but they linked and showed up in source branch.

I use CW 10.5.

 

Cheers!

 

9773_9773.jpgmulti-folder.jpg

ラベル(1)
0 件の賞賛
返信
1 返信

1,114件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

the simple way is to drag the folder from windows explore to the project folder in "CodeWarrior Projects" window directly. when you perform drag, CW will pop up message as below. you select the second or third. the folder link will be added to the project.

link folder to project.JPG.jpg

can this help?

0 件の賞賛
返信