Windows 7 crashes when building MQX libraries.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Windows 7 crashes when building MQX libraries.

ソリューションへジャンプ
3,226件の閲覧回数
VinceTF
Contributor III

Compilier:  CW Eclipse 10.2

RTOS:  MQX 3.8.1

Host OS: Windows 7 64 bit

 

Trying to build MQX libraries and windows crashes every time (get the blue screen, have to shut down).  Any idea what is causing this?

 

Also, I have noticed in task manager that the cwide process has a *32 next to it (see attachement).  I assume this means it is running in 32 bit mode.  Is this normal?

 

-Vince

ラベル(1)
0 件の賞賛
返信
1 解決策
3,135件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

I have seen cases where graphic card drivers can cause regular blue screens. Could you check if you have the latest and greatest graphic card drivers installed?

About 32bit: yes, that's normal. Actually a 64bit windows does not mean that everything is 64bit. Many applications run in 32bit mode. Only the device drivers have to be 64bit.

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,136件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

I have seen cases where graphic card drivers can cause regular blue screens. Could you check if you have the latest and greatest graphic card drivers installed?

About 32bit: yes, that's normal. Actually a 64bit windows does not mean that everything is 64bit. Many applications run in 32bit mode. Only the device drivers have to be 64bit.

Erich

0 件の賞賛
返信
3,135件の閲覧回数
VinceTF
Contributor III

Erich,

Thanks for the quick response!  I updated the drivers for my monitors and so far haven't seen the issue.

0 件の賞賛
返信