How to add new processor at existing project ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to add new processor at existing project ?

1,047件の閲覧回数
enzobruno
Contributor I

I have a working project maked with cw6.3 build 9279 + 6.3.1 patch build 10105 and using the processor MC9S08AW32.

I want to add new processor MS9S08AW16, without loosing the old one.

I have create a new Target with "create new target" and clone from existing target, but when attempt to change the processor type i have the error message "The change MCU feature is not available for project with more that one build target".

There is a solution ?

Thanx

ラベル(1)
0 件の賞賛
返信
0 返答(返信)