Why is file debugout.txt being created?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why is file debugout.txt being created?

ソリューションへジャンプ
1,968件の閲覧回数
frankbaird
Contributor III


I recently upgraded from CW 10.6.3 to 10.6.4 and now, every time I debug my program, the file debugout.txt is created at the top level of my workspace. Despite it being called a text file, it is clearly a binary file. Why is this file being created, and how do I stop it? If I can't stop it, how do I at least read and interpret it?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,842件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Frank,

could it be that you are using semihosting? In that case the target could write that file.

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,843件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Frank,

could it be that you are using semihosting? In that case the target could write that file.

Erich

0 件の賞賛
返信
1,842件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Fran,

Which chip do you used, could you please take a screenshot about the .txt file place.

Then i will check it .

BR

Alice

0 件の賞賛
返信
1,842件の閲覧回数
frankbaird
Contributor III

I am using the MCF52258 chip. The image below shows the file's location. I have attached the txt file as well.

pastedImage_0.png

0 件の賞賛
返信
1,842件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Frank,

Is the debugout.txt file created only when debugging that project? Could you share the project so we can reproduce it on our side?

Could you also tell us which programming interface are you using?

Thanks in advance!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 件の賞賛
返信