Which Codewarrior Edition for Kinetis and MPC55xx /MPC56xx

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Which Codewarrior Edition for Kinetis and MPC55xx /MPC56xx

跳至解决方案
1,629 次查看
ihsanyaz_c_
Contributor II

Hi,

 

Which edition of Codewarrior is suggested for use with both of Kinetis series and MPC55xx or MPC56xx?

We have two different projects and first of them is now in progress, with kinetis MCU but we are unhappy with KDS.

The other MPC project will start soon.

Can we use Codewarrior for both? If yes which edition (standard, prof.) ?

 

Thanks

标签 (1)
0 项奖励
回复
1 解答
1,479 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hi ihsan

Eclipse CodeWarrior for MCU supports most of Kinetis and all MPC56xx products. MPC55xx products are old and not supported in Eclipse CodeWarrior.

The latest version can be downloaded from:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10

For MPC55xx, please use the Classic CodeWarrior v2.10:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MPC55XX

For the difference of Basic Suite, Standard Suite and Professional Suite, please refer to:

http://www.freescale.com/files/soft_dev_tools/doc/fact_sheet/950-00437.pdf

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,480 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hi ihsan

Eclipse CodeWarrior for MCU supports most of Kinetis and all MPC56xx products. MPC55xx products are old and not supported in Eclipse CodeWarrior.

The latest version can be downloaded from:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10

For MPC55xx, please use the Classic CodeWarrior v2.10:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MPC55XX

For the difference of Basic Suite, Standard Suite and Professional Suite, please refer to:

http://www.freescale.com/files/soft_dev_tools/doc/fact_sheet/950-00437.pdf

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------