Where can I find source codes regarding floating point?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can I find source codes regarding floating point?

1,518 Views
lukekim
Contributor II

Here are our development environments.

- Window 7

- CodeWarrior v2.10 and CodeWarrior v10.7

 

I can find source codes and project files related to the default library at PowerPC_EABI_Support directory.

(ex : Runtime.PPCEABI.mpc ...)

But, I don't know where I can find source codes related to the floating point.

Please give me some information about that.

 

Thanks.

Labels (1)
0 Kudos
Reply
1 Reply

1,431 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

all source codes including header file, which are available for Power Architecture in CodeWarrior 10.7 are placed in installation folder/MCU/PA_Support. The same situation is for CodeWarrior 2.10. (there is also folder PowerPC_EABI_Support, where you can find some source codes)

Could you please more clarify, what do you mean by floating point?

Regards,

Martin

0 Kudos
Reply