Where can I find source codes regarding floating point?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where can I find source codes regarding floating point?

1,519件の閲覧回数
lukekim
Contributor II

Here are our development environments.

- Window 7

- CodeWarrior v2.10 and CodeWarrior v10.7

 

I can find source codes and project files related to the default library at PowerPC_EABI_Support directory.

(ex : Runtime.PPCEABI.mpc ...)

But, I don't know where I can find source codes related to the floating point.

Please give me some information about that.

 

Thanks.

ラベル(1)
0 件の賞賛
返信
1 返信

1,432件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hi,

all source codes including header file, which are available for Power Architecture in CodeWarrior 10.7 are placed in installation folder/MCU/PA_Support. The same situation is for CodeWarrior 2.10. (there is also folder PowerPC_EABI_Support, where you can find some source codes)

Could you please more clarify, what do you mean by floating point?

Regards,

Martin

0 件の賞賛
返信