What does CW put into S0 record?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What does CW put into S0 record?

跳至解决方案
1,448 次查看
kb3kj
Contributor I
I would like to know what information CW puts into the S0 record in
.S19 files. It seems to change when the project is recompiled in a different
directory, but not at different times in the same directory. My goal is to
make it so that others can compile the project and get exactly the same .s19
file.

I am using CW for the HC12 version 3.0

Jim
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
807 次查看
CompilerGuru
NXP Employee
NXP Employee
It's the filename of the elf file, I think.

For srecords creates with the burner, there is an option -Ns to configure if the full path or just the filename should be written to the s0, or if no s0 should be emitted at all.
However I don't know if this option is already in the V3.0 version you are using. Also srecords can be generated by other tools too (assembler/linker).

Daniel

在原帖中查看解决方案

0 项奖励
回复
1 回复
808 次查看
CompilerGuru
NXP Employee
NXP Employee
It's the filename of the elf file, I think.

For srecords creates with the burner, there is an option -Ns to configure if the full path or just the filename should be written to the s0, or if no s0 should be emitted at all.
However I don't know if this option is already in the V3.0 version you are using. Also srecords can be generated by other tools too (assembler/linker).

Daniel
0 项奖励
回复