Visualtization Tool - True Time Simulator

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Visualtization Tool - True Time Simulator

Jump to solution
2,302 Views
roberto_m
Contributor III

Hi,

I'm tryng to learn something on my HCS08 (QE64),
and I'm following step by step the AN2616.
I've defined LED4 PTCD_PTCD3.
It's a toggling led. I use true time simulator
and visualization tool. If I insert a simple LED
 instrument and port: Variable, eith Port to Display: LED4 it
 doesn't work for every bit (0,1,2..) I select.
 the only way to see it toggling is to set
 : memory, port to disdlay: PTCD. but in this case
 toggles also the other bits (when in data they still have the same value)
 Where I'm wrong?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,629 Views
CrasyCat
Specialist III

Hello

 

I do not really get what you are trying to do and how you are trying to do it.

It would probably be better to get one of our support engineer to look at this one.

I would recommend you to submit a service request for that.


Click here to submit a service request.

Make sure to attach a reproducible project and installed product information to the service request.
To generate the required information:
- Start CodeWarrior
- Open the project
- Select "Help" -> "Pack and Go" and follow instructions on the screen.

Attach the generated .zip file to the SR.

 

CrasyCat

View solution in original post

0 Kudos
Reply
1 Reply
1,630 Views
CrasyCat
Specialist III

Hello

 

I do not really get what you are trying to do and how you are trying to do it.

It would probably be better to get one of our support engineer to look at this one.

I would recommend you to submit a service request for that.


Click here to submit a service request.

Make sure to attach a reproducible project and installed product information to the service request.
To generate the required information:
- Start CodeWarrior
- Open the project
- Select "Help" -> "Pack and Go" and follow instructions on the screen.

Attach the generated .zip file to the SR.

 

CrasyCat

0 Kudos
Reply