Visualtization Tool - True Time Simulator

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Visualtization Tool - True Time Simulator

跳至解决方案
1,518 次查看
roberto_m
Contributor III

Hi,

I'm tryng to learn something on my HCS08 (QE64),
and I'm following step by step the AN2616.
I've defined LED4 PTCD_PTCD3.
It's a toggling led. I use true time simulator
and visualization tool. If I insert a simple LED
 instrument and port: Variable, eith Port to Display: LED4 it
 doesn't work for every bit (0,1,2..) I select.
 the only way to see it toggling is to set
 : memory, port to disdlay: PTCD. but in this case
 toggles also the other bits (when in data they still have the same value)
 Where I'm wrong?

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
845 次查看
CrasyCat
Specialist III

Hello

 

I do not really get what you are trying to do and how you are trying to do it.

It would probably be better to get one of our support engineer to look at this one.

I would recommend you to submit a service request for that.


Click here to submit a service request.

Make sure to attach a reproducible project and installed product information to the service request.
To generate the required information:
- Start CodeWarrior
- Open the project
- Select "Help" -> "Pack and Go" and follow instructions on the screen.

Attach the generated .zip file to the SR.

 

CrasyCat

在原帖中查看解决方案

0 项奖励
回复
1 回复
846 次查看
CrasyCat
Specialist III

Hello

 

I do not really get what you are trying to do and how you are trying to do it.

It would probably be better to get one of our support engineer to look at this one.

I would recommend you to submit a service request for that.


Click here to submit a service request.

Make sure to attach a reproducible project and installed product information to the service request.
To generate the required information:
- Start CodeWarrior
- Open the project
- Select "Help" -> "Pack and Go" and follow instructions on the screen.

Attach the generated .zip file to the SR.

 

CrasyCat

0 项奖励
回复