V3.1 Programming Algorithms SP trouble

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

V3.1 Programming Algorithms SP trouble

ソリューションへジャンプ
3,613件の閲覧回数
wre
Contributor III
I just installed the subject update that was announced in a recnet Freescale update e-mail.
 
Under the PEDebug menu of the True-Time debugger I am unable to select a device.  Or, more correctly, I can navigate through "Device: Unselected", to "68HC08", to "MR Family", to "HC08MR32", but as soon as I go back to the PEDebug menu, it shows "Device: Unselected".
 
This menu used to have an item to select the simulator or in-circuit debug but now is limited to:  Load..., Reset, Command Files, Device: Unselected and P&E Micro Hardware Documentation.
 
Any ideas what has happened?
 
Thanks,
 
Bill
 
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,908件の閲覧回数
wre
Contributor III

Just reinstalled the base software and the patches, including this latest one.  Everything seems to be working again.  Ticks me off that I had to go through that process though!

Bill

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,909件の閲覧回数
wre
Contributor III

Just reinstalled the base software and the patches, including this latest one.  Everything seems to be working again.  Ticks me off that I had to go through that process though!

Bill

 

0 件の賞賛
返信