Using crystal on DEMO board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using crystal on DEMO board

ソリューションへジャンプ
2,109件の閲覧回数
Iain
Contributor I

CW 5.9, HCS08QE32, DEMOQE

 

I wish to have a 1000Hz clock for TPM timing, and it was suggested by a forum member that that I should set my TPM to use 32kHz crystal XCLK, and prescaler of 32 to give me my 1000Hz clock, and that, I understand. 

Below is code I have to set the ICS (HCS08QE has no ICG).

 

 

ICSC1 = 0b10000000;  // CLKS = 10 external referenceICSC2 = 0b00000110;  // EREFS = 1 oscillator driving crystal,                     // ERCLKEN = 1 ICSERCLK enabledwhile(!ICSSC_OSCINIT){} // wait for external crystal to be initiallised

 

 

I am getting confused by internal/external references, there seems to be more options than I thought there would be, also the EREFS bit I am unsure of, as the book I am using and data sheet seem to contradict each other when mentioning oscillators/crystals/resonators.

 

Basically I just want to set the micro to make use of the 32kHz crystal on my demo board (attatched to EXTAL and XTAL pins),  but am not sure if I am setting the registers correctly, can anyone help?

 

Regards,

Iain

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,576件の閲覧回数
bigmac
Specialist III

Hello Iain,

 

I had a closer look at the ICS section in the reference manual, and the fixed frequency clock source is derived differently compared with some of the other HCS08 devices.  For the QE device, the fixed frequency clock, as an alternate clock source for the TPM modules, is derived from the current reference source, whether internal or divided external source.  For other devices, the external source is used.  This means that it would seem possible to use either FEI mode or FEE mode to generate the bus frequency, and also provide the alternate TPM clock.

 

I also see that there is an additional frequency division by 2, before the clock is applied to the TPM prescaler, that I had previously overlooked. This means that the clock frequency will be nominally 16 kHz.

 

Accepting that you still require to use an external reference, I believe that the ICSC1 value should be 0x00 in order to source the bus clock from the FLL.  A setting of 0x80 would be causing FBE mode, giving a 16 kHz bus frequency  - not what you require.   A nominal bus frequency of 4 MHz should be achieved with ICSC2 = 0x44; and ICSSC = 0x00;

i.e. Bus frequency = 32768 * 512 / 2 / 2

 

Regards,

Mac

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,577件の閲覧回数
bigmac
Specialist III

Hello Iain,

 

I had a closer look at the ICS section in the reference manual, and the fixed frequency clock source is derived differently compared with some of the other HCS08 devices.  For the QE device, the fixed frequency clock, as an alternate clock source for the TPM modules, is derived from the current reference source, whether internal or divided external source.  For other devices, the external source is used.  This means that it would seem possible to use either FEI mode or FEE mode to generate the bus frequency, and also provide the alternate TPM clock.

 

I also see that there is an additional frequency division by 2, before the clock is applied to the TPM prescaler, that I had previously overlooked. This means that the clock frequency will be nominally 16 kHz.

 

Accepting that you still require to use an external reference, I believe that the ICSC1 value should be 0x00 in order to source the bus clock from the FLL.  A setting of 0x80 would be causing FBE mode, giving a 16 kHz bus frequency  - not what you require.   A nominal bus frequency of 4 MHz should be achieved with ICSC2 = 0x44; and ICSSC = 0x00;

i.e. Bus frequency = 32768 * 512 / 2 / 2

 

Regards,

Mac

 

0 件の賞賛
返信