Using Visualization Tool with ADC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using Visualization Tool with ADC

2,582件の閲覧回数
manishk
Contributor I
Hi,
    I am using the HCS08(QG), and I have configured the ADC in 'Continous Sample Mode' and its using the Bus Clock of 4.1 MHz.

    But when I use the Visualization Tool to plot the ADC input, I get around 3 samples per second. Is it a limitation with the Visualization Tool or am I doing something wrong?


Message Edited by manishk on 2007-11-13 11:14 AM
ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,475件の閲覧回数
CrasyCat
Specialist III
Hello
 
I assume you have added a Chart Instrument to your Visualization tool component. Am I right?
 
You can adjust the "Unit Size" to get a smaller period, but keep in mind that if the period is too small there will be a lot of communication through the BDM connection and your application might not run in real time any more.
 
CrasyCat

1,475件の閲覧回数
manishk
Contributor I
Thanks a lot for your reply :smileyhappy:.

Yes, I have added the Chart Instrument.

Is there a way I can find out how small I can keep the peroid, while still staying within the limits of real-time?

I'm using Device Initialization Expert to configure the ADC. It shows a certain value for the conversion time, is it the effective sample  rate or just a theoretical value?
0 件の賞賛
返信