Hi i am trying to measure a Memsic 2125 accelerometer, (measuring the pulse width) and i am using a Adapt9s12e128 board with a MC9S12E128, i am trying to use this code, but it seems that the isr is not working or that it's not doing anything (the accelerometer has 2 channels, but they are the same just differ on the axis, so if one works it's easy to make the other0
this is the code i am using, i hope you can help me find the error (the oscillator freq is 24 MHz via PLL)
ORG RAMStart
; Insert here your data definition.
org $3000
cnt dc.w 0
trans dc.w 0
per dc.w 0
posx dc.w $0
; code section
ORG ROMStart
Entry:
_Startup:
;bus 24/2=12Mhz T=1/12Mhz=.083333 us, overflow en 5461.33 us => 5.46133 ms = 183 Hz ov
;LDS #RAMEnd+1 ; initialize the stack pointer
movb #$90, TIM1_TSCR1 ;timer,banderas rapidas
movb #0, TIM1_TSCR2 ;no int ov, no presc
movb #$e0, TIM1_TIOS ;1 capturas c0
movb #1, TIM1_TCTL3 ;1 capt tran pos #5
movb #$10,TIM1_TIE ;int 1 capt #$30
movb #$ff,TIM1_TFLG1 ;borra banderas
movw #$ffff,DDRAD
movw #$ffff,ATDDIEN
movb #1,DDRP ;salida led rojo
cli
;sensor 100 Hz PWM 50% dtcy = 0g 100Hz=10ms=10,000us
;form= |`TH`|_TL_| Tx=periodo F=TH/Tx
main:
bset PTP,mPTIP_PTIP0
movw posx,PTAD
bra main
medicionx:
sei
ldd TIM1_TCNT ;borr band
std trans
movb #2,TIM1_TCTL3; config timer trans baja
brclr TIM1_TFLG1,mTIM1_TFLG1_C4F,*
ldd TIM1_TCNT
std per
subd trans ;long
std posx ;tiempo
movb #1,TIM1_TCTL3
cli
rti
;**************************************************************
;* Interrupt Vectors *
;**************************************************************
ORG $FFFE
DC.W Entry ; Reset Vector
org Vtim0ch4
dc.w medicionx
解決済! 解決策の投稿を見る。
well i got it working, i had to change to the timer0, i dont know why timer1 never worked (i had set up the tim0 int vector first but changing it to tim1 didn't work either) but now it does display the value on the led's, but they are always changing even if the accelerometer us still, so am i making any mistakes on the operations? or is it something else
ldd TIM1_TCNT ;borr band
This doesn't clear capture flag in TFFCA=1 mode. Please read TFFCA description. You need to clear capture flags twice in your ISR. Instead of reading TCNT you should read your capture TCx register.
You shouldn't sei and cli in ISR, since MCU does it automatically on entry and on exit from ISR.
well i modified the code as you suggested and it still doesnt work, nothing is being displayed on the led's connected to PTAD, i changed the code to this
medicionx:
ldd TIM1_TC4 ;borr band
bset TIM1_TFLG1,mTIM1_TFLG1_C4F
std trans
movb #2,TIM1_TCTL3; config timer trans baja
brclr TIM1_TFLG1,mTIM1_TFLG1_C4F,*
ldd TIM1_TC4
bset TIM1_TFLG1,mTIM1_TFLG1_C4F
std per
subd trans ;long
std posx ;tiempo
neg posx
movb #1,TIM1_TCTL3
rti
i also cleared the falg by writing one to the corresponding bit
I don't know why, maybe because you don't initialize stack pointer, maybe there are other reasons. But
bset TIM1_TFLG1,mTIM1_TFLG1_C4F
1) All writes to TFLG1 are ignored in TFFCA=1 mode.
2) In TFFCA=0 mode above line will clear ALL TFLG1 flags. To clear just C4F you need to either
movb #mTIM1_TFLG1_C4F, TIM_TFLG1
or
bclr TIM1_TFLG1, #~mTIM1_TFLG1_C4F
well i got it working, i had to change to the timer0, i dont know why timer1 never worked (i had set up the tim0 int vector first but changing it to tim1 didn't work either) but now it does display the value on the led's, but they are always changing even if the accelerometer us still, so am i making any mistakes on the operations? or is it something else