Use CW 10.6 to debug SPC5668E

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Use CW 10.6 to debug SPC5668E

1,498 次查看
jonasa
Contributor III

Hello,

 

I'm looking for a good alternative to debug the PowerPC microcontroller SPC5668E. One alternative would be to use CW 10.6 together with P&E Micro's debug probe (U-MULTILINK or U-MULTILINK-FX).

 

Does anyone have experience with this setup?

I would also like to know if an 14-Pin Berg to 38-Pin Mictor Adaptor (like http://www.pemicro.com/products/product_viewDetails.cfm?product_id=159  ) is included if I buy U-MULTILINK or U-MULTILINK-FX? I have a 38-pin mictor on the PCB.

What debug features are included in CW 10.6?

Can I set a breakpoint while the programming is running?

Can I get live update on variables?

Callstack?

Can I change variables etc.?

Write to HW registers?

Is trace included?

Can I program the device with CW 10.6?

 

Kind regards,

Jonas

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

1,350 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello Jonas

It is a same question with this one:

Use CW 10.6 to debug SPC5668E

Best Regards

Fiona Kuang

Technical Information & Commercial Support

0 项奖励
回复