Unable to add SVN: problems with Mylyn

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to add SVN: problems with Mylyn

3,009件の閲覧回数
RobertoPaolinel
Contributor II

Dear all,

I'm working with HCS08SG32 and I tried to add SVN support to my CW 10.6.4. Build Id:150416.

 

CW 10.6. does not have Eclipse Marketplace so I looked for SVN plugin update site, both subclipse and subversive, but no installation was ok because of missing Mylyn integration.

So I looked for Mylyn and I tried with both 3.19 and 3.8, but there's always some missing dependency.

 

How can I come out of it?

 

Thank you very much in advance for your kind reply.

Best Regards

Roberto

ラベル(1)
3 返答(返信)

2,758件の閲覧回数
RobertoPaolinel
Contributor II

Thank you Alice!

Subclipse 1.8 installation was fine!

But anyway I got this error when I right clicked on Project / Team /Share Project /SVN

org.apache.subversion.javahl.ClientException: Unsupported working copy format

svn: This client is too old to work with the working copy at

'C:\Users\roberto.paolinelli\Progetti\CNH\SAFETY\Code\trunk' (format 31).

You need to get a newer Subversion client. For more details, see

  http://subversion.apache.org/faq.html#working-copy-format-change

Since I was not able to solve the problem with eclipse I started versioning with using Tortoise SVN client.

TortoiseSVN 1.9.4, Build 27285 - 64 Bit , 2016/04/24 13:59:58

Subversion 1.9.4, -release

This SVN version is supported by Subclipse 1.12 but I'm afraid I will meet same problems as before.

I will let you know.

Best Regards

Roberto

0 件の賞賛
返信

2,758件の閲覧回数
RobertoPaolinel
Contributor II

Just to update that with subclipse 1.12 it's all OK now, but just after having installed 1.8 first as Alice suggested me.

Thank you very much Alice!

0 件の賞賛
返信

2,758件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Roberto,

Please test this:

Click "Help" "Install new software" Click "Add" to add the site URL "http://subclipse.tigris.org/update_1.8.x"

pastedImage_1.png

After install it , you can refer to this thread to use SVN :

How to install support for Subversion on 10.6.4 (latest CW)

Also you can use GIT to control your project version:

https://mcuoneclipse.com/2013/08/13/installing-egit-in-eclipse-and-codewarrior-for-mcu10-4/

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------