USBDM 4.12.1.30 ARM Programmer Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USBDM 4.12.1.30 ARM Programmer Issue

1,926件の閲覧回数
diegovalerio
Contributor II

Hello Everybody.

I have some issues using the USBDM 4.12.1.30 ARM Programmer.

I am working with a MKE02Z64M2 chip, and I am trying to program its Flash with the ARM Programmer, but I have communication errors when I introduce my programmed device in my system.

I generate the .s19 file with CW 10.6 following the next steps:

   1. I enabled the option to Create Flash Image, with the Output format srec.

   2. I compiled the program. I have the ProjName.hex file.

   3. I copied the .hex file in the Computer Desktop and renamed it as ProjName.s19.

Then, with USBDM 4.12.1.30 ARM Programmer, I loaded the .s19 file. I selected the Device and Clicked Detect Chip.

In security I checked Image and in programming Erase Mode "Erase All" is selected.

Then, I clicked Program Flash. It has no errors. 

When I introduce the device in my system, the communication gets wrong.

As when I debug in CodeWarrior, I can specify the Trim Options, ant it does not generate any trouble with the communication.

pastedImage_4.png 

pastedImage_5.png

I think this is something that generates the trouble with my UART communication. In the USBDM ARM Programmer, I can't specify those values:

pastedImage_7.png

The program loads correctly in the device, but when it tries to establish serial communication through its UART port, a lot of communication error occurs, but when I compiled it with CodeWarrior through a PEMicro Debbuger, the serial communication works fine. Hope I made my point clear.

Could somebody help me with this? I need to be able to load .s19 files to my ARM devices with no errors like this one.

Best Regards,

Diego.

タグ(5)
0 件の賞賛
返信
1 返信

1,719件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Diego Valerio,

Does your project includes the code like printf to console , or other debug code ?

If yes, when flash it to chip , the project can't work well.

So could you please first test a simple project , like only a gpio (LED)  ?

BR

Alice

0 件の賞賛
返信