USB License Dongle

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,329件の閲覧回数
msulli
Contributor I
I just got a USB License dongle for CodeWarior.  But MultiLink that CodeWarrior programs HCS08 BDM also uses USB.  My laptop has one USB, and I want be able to re-program HCS08 using CodeWarrior and USB MultiLink at customer site, by portable license transfer from Desktop computer to Laptop.  Has anyone experience with this?  Can this be accomplished with one USB port on a Laptop ? Do I need some kind of 2 to 1 USB splitter (there is no plug on the back of the USB dongle to plug the USB MultiLink into,... like some parallel port dongles do..) .  Once I get CodeWarrior running, will the computer recheck for the dongle if I pull it out and plug in the USB MultiLink ? ....    Thanks...   Mark
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,481件の閲覧回数
alex_spotw
Contributor III
Hi:

What you need is a USB Hub, that will wive you several USB ports out of one USB connection in the laptop. You can buy them very cheap for $20-$30 anywhere, even Wal-Mart sells them.

Regards,

Alex

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,482件の閲覧回数
alex_spotw
Contributor III
Hi:

What you need is a USB Hub, that will wive you several USB ports out of one USB connection in the laptop. You can buy them very cheap for $20-$30 anywhere, even Wal-Mart sells them.

Regards,

Alex
0 件の賞賛
返信