UART TX interrupt not occured

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART TX interrupt not occured

ソリューションへジャンプ
2,175件の閲覧回数
olegivanus
Contributor III

Hello everyone,

Why does UART not cause interrupt handler?

Look at my project below

Thank you!

Original Attachment has been moved to: UART.zip

ラベル(1)
0 件の賞賛
返信
1 解決策
1,881件の閲覧回数
Rick_Li
NXP Employee
NXP Employee

Hi Oleg,

the silicon you are using is MPC5643, I have forward this issue to my another colleague and she will help you on it!

Regards,

Yong

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,881件の閲覧回数
Rick_Li
NXP Employee
NXP Employee

Hello Oleg,

I'm sorry, could you please re-upload your UART.zip?

The project you attached can't be downloaded!

0 件の賞賛
返信
1,879件の閲覧回数
olegivanus
Contributor III

Hello, Yong Li

See attachment below)

Thanks

0 件の賞賛
返信
1,882件の閲覧回数
Rick_Li
NXP Employee
NXP Employee

Hi Oleg,

the silicon you are using is MPC5643, I have forward this issue to my another colleague and she will help you on it!

Regards,

Yong

0 件の賞賛
返信
1,879件の閲覧回数
olegivanus
Contributor III

Thank you!

0 件の賞賛
返信