Trying to Copy a Processor Expert Project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Trying to Copy a Processor Expert Project

ソリューションへジャンプ
2,211件の閲覧回数
rsk2
Contributor I

Hello,

 

I have developed a C project using Processor Expert and now I would like to copy this project. (I have the same processor with the mostly the same functionality on two different boards). I tried copying the folder and renaming some files, but the PE settings did not get transfered. Is there a tool to handle moving the PE settings?

Thank you,
Randy

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,847件の閲覧回数
ProcessorExpert
Senior Contributor III

Hello,

 

I am guessing that you are using CodeWarrior Classic, because you have not mentioned this information in your post.

 

I think that the easiest way will be the following (this steps also match for renaming a project without point 4):

 

1- Create new PE Project with MCU that you use

2 - Using “Import…” menu command import all PE settings from origin project (import menu command is available in pop-up menu of "Project Panel" window by clicking into white space)

3 - Copy Events.c, Events.h, and main module from origin project into new one (eventually also user modules)

4 - Set PE components according to another PCB

 

best regards
Vojtech Filip
Processor Expert Support Team

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,848件の閲覧回数
ProcessorExpert
Senior Contributor III

Hello,

 

I am guessing that you are using CodeWarrior Classic, because you have not mentioned this information in your post.

 

I think that the easiest way will be the following (this steps also match for renaming a project without point 4):

 

1- Create new PE Project with MCU that you use

2 - Using “Import…” menu command import all PE settings from origin project (import menu command is available in pop-up menu of "Project Panel" window by clicking into white space)

3 - Copy Events.c, Events.h, and main module from origin project into new one (eventually also user modules)

4 - Set PE components according to another PCB

 

best regards
Vojtech Filip
Processor Expert Support Team

 

0 件の賞賛
返信