The Problem that the Codewarrior V4.5 generating the .phy file for HCS12X family

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The Problem that the Codewarrior V4.5 generating the .phy file for HCS12X family

ソリューションへジャンプ
2,308件の閲覧回数
xingzou
Contributor I
When I use the Codewarrior V4.5 to compile  the project for MC9S12XDT512 MCU, the .phy file generated  in the /bin directory is wrong, which is different from the file generated by  log2Phy_12.exe. I think the Codewarrior V4,5 still use the way of HCS12 for HCS12X. In fact, the memory managemant between HCS12 and HCS12X is very different.
 
Whether I need configue the CW V4.5 for getting the right .phy file.
Thanks.
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,469件の閲覧回数
CrasyCat
Specialist III
Hello
 
If you create a project for HCS12X using the project wizard, the .bbl file generated will generate:
  a file with extension .abs.s19, which contains S records with logical (non - linear) addresses
  a file with extension .abs.glo, which contains S records with global addresses.
 
The delivered default.bbl file does not generate any S record file with physical addresses.
 
CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,470件の閲覧回数
CrasyCat
Specialist III
Hello
 
If you create a project for HCS12X using the project wizard, the .bbl file generated will generate:
  a file with extension .abs.s19, which contains S records with logical (non - linear) addresses
  a file with extension .abs.glo, which contains S records with global addresses.
 
The delivered default.bbl file does not generate any S record file with physical addresses.
 
CrasyCat
0 件の賞賛
返信