Hi,
I have a stupid question on define pin.
I want define the name of pin, example:
char SdaPin;
SdaPin= PTCD_PTCD2;
but when I write:
SdaPin= 1;
this not work!!!
Sorry for stupid question, I don't understand!!!
Thanks
 
					
				
		
Thanks but...With variable it's impossible?
I used 3 pin for i2c (manual i2c not with dedicated function).
I have make generic Start, Stop,Write, Read. Before I use this function I set my port, example:
char SdaPin;
SdaPin= PTCD_PTCD2;
Start();
Write();
Stop();
//other pin
SdaPin= PTCD_PTCD3;
Start();
Write();
Stop();
This is impossible if I must use a DEFINE.
I must re-write my function, one for each pin? Example:
Start_Pin2();
Write_Pin2();
Stop_Pin2();
and
Start_Pin3();
Write_Pin3();
Stop_Pin3();
Thanks again!!
Yes, it is possible to use it as a variable, but it's not as efficient as macro that generates just single bit set/clear instruction. On the other hand you can reuse the functions easily:
e.g.:
#define PIN_ON(x) *##x##.reg |= ##x##.mask
#define PIN_OFF(x) *##x##.reg &= ~##x##.mask
typedef struct {
 char *reg;    // poitner to the register
 char mask;    // bit mask
} tReg;
tReg SDA1 = {&PTADD, PTADD_PTADD0_MASK};   // define register address and particular bit(s)
tReg SDA2 = {&PTADD, PTADD_PTADD1_MASK};
void main(void)
{
  PIN_ON(SDA1);
  PIN_OFF(SDA1);
  PIN_ON(SDA2);
  PIN_OFF(SDA2);
}Disassembly listing:
21: PIN_ON(SDA1); 0001 c60002 [4] LDA SDA1:2 0004 320000 [5] LDHX SDA1 0007 fa [3] ORA ,X 0008 f7 [2] STA ,X 22: PIN_OFF(SDA1); 0009 c60002 [4] LDA SDA1:2 000c 43 [1] COMA 000d 320000 [5] LDHX SDA1 0010 f4 [3] AND ,X 0011 f7 [2] STA ,X 23: 24: PIN_ON(SDA2); 0012 c60002 [4] LDA SDA2:2 0015 320000 [5] LDHX SDA2 0018 fa [3] ORA ,X 0019 f7 [2] STA ,X 25: PIN_OFF(SDA2); 001a c60002 [4] LDA SDA2:2 001d 43 [1] COMA 001e 320000 [5] LDHX SDA2 0021 f4 [3] AND ,X 0022 f7 [2] STA ,X
Using register macros will generate more efficient code:
void main(void)
{
  PTADD_PTADD0 = 1;
  PTADD_PTADD0 = 0;
  PTADD_PTADD1 = 1;
  PTADD_PTADD1 = 0;
}Disassembly listing:
27: PTADD_PTADD0 = 1; 0001 1000 [5] BSET 0,_PTADD 28: PTADD_PTADD0 = 0; 0003 1100 [5] BCLR 0,_PTADD 29: 30: PTADD_PTADD1 = 1; 0005 1200 [5] BSET 1,_PTADD 31: PTADD_PTADD1 = 0; 0007 1300 [5] BCLR 1,_PTADD
Stanish
stanish wrote: Using register macros will generate more efficient code:
Hello,
If you require that each function make use of a choice of SDA pins, you will need to pass this choice to each of the functions. Assuming that all the pins are allocated to PTCD, you might have something like the following -
#define SDA2 2
#define SDA3 3
// Bit manipulation macros:
#define  bset(n,reg)   (reg) |= (1 << (n))
#define  bclr(n,reg)   (reg) &= ~(1 << (n))
void Start( byte bitnum)
{
bset( bitnum, PTCD);
  ...
...
bclr( bitnum, PTCD);
}
void main( void)
{
for ( ; ; );
Start( SDA2);
...
Start( SDA3);
    ...
 
}
}
Regards,
Mac
Hello,
Using the preprocessor macro -
#define SdaPin PTCD_PTCD2
should permit SdaPin = 1; to be used.
Whenever the symbol SdaPin is encountered, the preprocessor will substitute PTCD_PTCD2. As it happens, this is also a macro (defined in the derivative header file), so a further substitution will actually take place.
Regards,
Mac