Storing in PC RAM content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Storing in PC RAM content

Jump to solution
3,226 Views
mmm
Contributor I

I have a 9S08QG8 microcontroller, with the demo board connected by USB with my PC. I'm doing some programs, but I don't know how to store the memory (some directions of the RAM) in my PC. Can I do it? and how?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,173 Views
stanish
NXP Employee
NXP Employee

KATBACK,

 

There is the command "SAVE" you can enter into Debbugger Command Line Window. e.g:

 

in>save 0x0080..0x008F my_memory_dump.s19

 

The debugger creates file my_mem_dump.s19 directly in your project directory and contains memory block 0x0080 - 0x008F.

 

See attached screenshot.

 

Stanish

View solution in original post

0 Kudos
Reply
3 Replies
2,173 Views
stanish
NXP Employee
NXP Employee

KATBACK,

 

You can use the debugger to store the memory content into the file e.g. command "SAVE".

If you need to capture data in the runtime there is a free tool called FreeMASTER

 

Stanish

 

Message Edited by stanish on 2009-02-27 11:44 AM
0 Kudos
Reply
2,173 Views
mmm
Contributor I

Thanks Stanish.

With "Save" command in the debugger, It doesn't save the content, it saves the windows configuration and position. Or if it also saves the content, in which file does it save?

Message Edited by KATBACK on 2009-03-02 02:49 PM
0 Kudos
Reply
2,174 Views
stanish
NXP Employee
NXP Employee

KATBACK,

 

There is the command "SAVE" you can enter into Debbugger Command Line Window. e.g:

 

in>save 0x0080..0x008F my_memory_dump.s19

 

The debugger creates file my_mem_dump.s19 directly in your project directory and contains memory block 0x0080 - 0x008F.

 

See attached screenshot.

 

Stanish

0 Kudos
Reply