Storing data to flash in k20d72m

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Storing data to flash in k20d72m

900件の閲覧回数
josephxavier
Contributor III

please share me a code to store data to flash (my need is to retain data even after power off ) , I am using K20D72M development kit.

what is the starting address for user data to be stored in flash?

ラベル(1)
0 件の賞賛
返信
1 返信

819件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello josephxavier:

Thank you for posting this question.

If you intend to use the FlexNVM functionality to store data, then in the next discussion you can find an example project attached to the response of colleague Carlos Casillas:

Re: FlexNVM Read/Write?

There is an application note to understand the whole FlexMemory system (AN4282) and the address space to be used:

http://cache.nxp.com/files/32bit/doc/app_note/AN4282.pdf

I hope this information is helpful.


Best Regards!
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信