Specify Memory Location for Comms Driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Specify Memory Location for Comms Driver

ソリューションへジャンプ
1,792件の閲覧回数
jimfell
Contributor III

I'd like to specify a memory location for a USB driver.  I've compiled the Freescale USB stack (v4.0.2) as a library, and I'd like to specify the memory location, so that the driver can be shared between main code and the boot loader.  What's the best way to do this?  I imagine that there would have to be a mechanism to map functions to the appropriate call address.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,703件の閲覧回数
BlackNight
NXP Employee
NXP Employee

You need to do this with the linker file. Basically marking the functions in the source file with an attribute (segment name), and then place the functions into a memory area in the linker file.

The syntax is somewhat different from compiler to compiler (and linker to linker).

Hope this helps,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,704件の閲覧回数
BlackNight
NXP Employee
NXP Employee

You need to do this with the linker file. Basically marking the functions in the source file with an attribute (segment name), and then place the functions into a memory area in the linker file.

The syntax is somewhat different from compiler to compiler (and linker to linker).

Hope this helps,

Erich

0 件の賞賛
返信