Setting Output Compare with MC9S12C32

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting Output Compare with MC9S12C32

Jump to solution
2,578 Views
maurix1966
Contributor I
Hello!
 
I'm new with Freescale.
I've a problem with a MC9C12C32.
The question is:
how i can set , with processor expert, a pin to be an output compare?
 
I've tried with Processor Expert and i can only set a pin to be an Input Capture but not Output Compare.
 
Thank you for help.
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,771 Views
CrasyCat
Specialist III
Hello
 
I have created a project for HCS12C32 and if I add a "TimeOut" Bean, I am able to define PT0_PWM0_IOC0 as output pin.
 
I am using CodeWarrior for HC12 V4.5
 
CrasyCat

View solution in original post

0 Kudos
Reply
1 Reply
1,772 Views
CrasyCat
Specialist III
Hello
 
I have created a project for HCS12C32 and if I add a "TimeOut" Bean, I am able to define PT0_PWM0_IOC0 as output pin.
 
I am using CodeWarrior for HC12 V4.5
 
CrasyCat
0 Kudos
Reply