Setting Conditional Breakpoint on Program Counter

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting Conditional Breakpoint on Program Counter

2,764 Views
jimfell
Contributor III

My embedded application (on MCF51JM128) is crashing for some unknown reason.  When the debugger finally breaks, usually on an access violation or invalid instruction, the stack is so badly corrupted that it does not provide any useful debugging information.  If possible, I'd like to set a conditional breakpoint on the Program Counter (PC), so that whenever it is set outside the valid range of addresses in which our application resides in Flash it will trigger a break.

 

I am using CodeWarrior 10.2, and so far I've found what looks like a mechanism for implementing a conditional break on the PC (see attached images).  How should I configure the Set Trigger Properties dialog box to setup the breakpoint?  Our application's valid range of addresses is between 0x00000420 and 0x00006628.  Thanks!

Labels (1)
0 Kudos
Reply
0 Replies