Saving the Data:1 HC(S)12(X) Debugger window to a .TXT (or .CSV) file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Saving the Data:1 HC(S)12(X) Debugger window to a .TXT (or .CSV) file

ソリューションへジャンプ
1,529件の閲覧回数
aceshigh99
Contributor I

Is there any way to halt the debugger, and dump all of the variable data contained in the Data:1 window to some sort of .TXT file, or CSV, etc.?

 

I can't seem to find any way to do it, and using alt-prntscrn to paste a pic of the data window into Powerpoint is tedious, to say the least.

 

Also, is there any way to expand the content of ALL structures in the Data:1 window, instead of having to manually click the for each one?  I have some large arrays for data logging, and it really slows down the debugging process to expand each structure one-by-one.

 

Thanks in advance for the help.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,014件の閲覧回数
CrasyCat
Specialist III

Hello

 

You can dump content of Data:1 window using the Command

      Data:1 < DUMP

If you want to store the Data window dump to a file use the commands:

 

      LF DataDump.txt

      Data:1 < DUMP

      NOLF

 

Please Refer to Debugger_HC12.pdf BOOK IV for more information on the available commands.

 

I am not aware of a simple way to expand all structure variable in the Data window.

 

CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,015件の閲覧回数
CrasyCat
Specialist III

Hello

 

You can dump content of Data:1 window using the Command

      Data:1 < DUMP

If you want to store the Data window dump to a file use the commands:

 

      LF DataDump.txt

      Data:1 < DUMP

      NOLF

 

Please Refer to Debugger_HC12.pdf BOOK IV for more information on the available commands.

 

I am not aware of a simple way to expand all structure variable in the Data window.

 

CrasyCat

0 件の賞賛
返信