SWI and SYS interrupts configuration in processor export

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SWI and SYS interrupts configuration in processor export

4,084 次查看
rajesh057
Contributor III

I have generated SWI and SYS interrupts using processor export

->In modules ->vector table ->Vsys,Vswi configured and code generated .while building code its saying functions undefined in Vswi.c file contain definition but its commented ..is their any problem to create Vswi,Vsys.

if no can pls help me to crate interrupts and code generation

Thanks

Rajesh

0 项奖励
回复
8 回复数

3,848 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Rajesh,

Could you tell us which MCU are you using?

Thanks in advance!

Best Regards,
Carlos Mendoza
Technical Support EngineerRajesh

0 项奖励
回复

3,848 次查看
rajesh057
Contributor III

Hi Carlos,

I am using MC9S12ZVC192 MICRICONTOLLER and code warrior tool .

Thanks,

Rajesh Kota

0 项奖励
回复

3,848 次查看
rajesh057
Contributor III

Hi Carlos,

Hi can I get what and all cover under SYS interrupt and SWI interrupt ..any special document on sys and swi apart data sheet and Instruction set.

Thanks ,

Rajesh Kota

0 项奖励
回复

3,848 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Rajesh,

You can enable these two interrupts  in CPU properties. then generate pe code, you will see the related vector and  interrupt function generated. See attached video.

pastedImage_1.png


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

3,848 次查看
rajesh057
Contributor III

1.GIF

2.GIF

4.GIF

5.GIF

Hi pls find the above pics I can able create interrupts from components ...but ur suggestion in cpu component inspector is it both are same .

S12zvc have any core self test functionality check .on of the document saying having SCST module for S12ZVC.

Thanks ,

Rajesh Kota

0 项奖励
回复

3,848 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Rajesh,

I believe your last two screenshots are generated by component InterruptVector. Something like Vsys.c. Vswi.c

In CW10, these c files from InterruptVector component  are commented. To use the generated functions, we need manually copy them for example

pastedImage_1.png

to User modules:

main.c
or

Events.c

These are also suggested under comments.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

3,848 次查看
rajesh057
Contributor III

Hi Jennie ,

1)My question is Both process of creating interrupts different but result is it same ?

2)Core self test component is avail for S12Zvc if its is yes can you pls give me over view of Self test module .

thanks

Rajesh Kota

0 项奖励
回复

3,848 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Rajesh Kota

Regarding to your questions:

>>1)My question is Both process of creating interrupts different but result is it same ?

Answer: Correct.

>>2)Core self test component is avail for S12Zvc if its is yes can you pls give me over view of Self test module .

Answer: I don't think we have core self test component.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复