SC56f8034 with USBDM_CF

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SC56f8034 with USBDM_CF

3,153件の閲覧回数
shgatev
Contributor I

Hi, I need to read Nick's sc56f8034 with usbdm_cf tool, can someone help me with connection diagram and how to do it, I am not familiar with this programmer, thanks

タグ(1)
0 件の賞賛
返信
3 返答(返信)

3,001件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Simeon,

I have never heard the SC56F8034, there is not any reference manual and data sheet on the NXP public website, I suppose that the SC56F8034 is customized DSC processor, which is confidential for the User manual, data sheet even customer information. If it is customized product for special customer, I am sorry, I can not support, because I have not any documentation and knowledge.

BR

Xiangjun Rong

0 件の賞賛
返信

3,001件の閲覧回数
shgatev
Contributor I

Thanks for your reply, you are right I cannot find any information, it's  ok but for me is interesting to know how to connect programmer, for example to MC56f8033 this mcu is in list of programmer, if you can help.

Thanks

0 件の賞賛
返信

2,998件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Simeon,

This is only my guess, I suppose that the SC56F8033/34 is similar with MC56F8037 from name, I attach the schematics of MC56F8037EVM, you can use USBTAP device to connect to the 14 pins JTAG connector on the PCB of MC56F8033/34.

Note this is only guess, I do not ensure it is correct, because I have not any inf about the customized product.

USBTAP link:

USB TAP for ONCE DSC | NXP 

BR

XiangJun Rong

0 件の賞賛
返信