S12ZVM CW11.1 internal compiler error - report to cw_bug@freescale.com

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12ZVM CW11.1 internal compiler error - report to cw_bug@freescale.com

1,376件の閲覧回数
raja1999
Contributor II

Hello,

I am getting error on ending line of a function (at closing curly brace).

Here's my error:

<fileName>.c|1677|0|1|91472|1)
=}
>internal compiler error (report to <cw_bug@freescale.com>)
>while executing in file 'ExpandIR.c' line: 7135
>(compiling '<functionName>' in '<fileName>.c')

Errors caused tool to abort.
NMAKE : fatal error U1077: '"C:\Freescale\CW MCU v11.1\MCU\S12lisa_Tools\Build_Tools\mwccs12lisa.exe"'
: return code '0x1'
Stop.
NMAKE : fatal error U1077: 'C:\apps\Nmake\nmake.EXE' : return code '0x2'
Stop.

 

Usually compiler lay out their concerns for our code. But this one just tells line no.! Installed it today.

P.S: I emptied out function, the error vanished.

Also, I changed compiler optimization level from 2 to 0, it worked. No error. Any opt level except 0 generates error.

P.S: I am using evaluation version of compiler (awaiting license from customer). Is this error because of any free eval limit?

Thanks

タグ(2)
0 件の賞賛
返信
1 返信

1,369件の閲覧回数
raja1999
Contributor II

bump!

anyone?

0 件の賞賛
返信