S12Z CW10.6  Floating point using

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12Z CW10.6  Floating point using

3,700件の閲覧回数
ahnjoseph
Contributor III

last,I had build project that was not to select  option of floating point

Now i need floating point calculation

so i want to modify project

 

i know it can new build project select floating point

But i need just modify last project

Can i this it ? 

ラベル(1)
2 返答(返信)

3,308件の閲覧回数
ahnjoseph
Contributor III

Hi ~~Jorge_Gonzalez<http://jiveon.jivesoftware.com/mpss/c/sAA/PDcDAA/t.1ok/sHX7M9b1TLSy4gna7wYGzw/h1/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQgIipR7LSY7eTtVAcgJLE9lLRbSJqskDy6gAq8WkKb-2Br4mmseyPVn6s9PlzYnOL68-3D>

Thanks your support

Your guide is perfect

So, Clear My problem

How can I select correct answer?

Perhaps My Company Computer is protect by IT team

So, I will re-tri it with my personal computer

Have a good Weekend

Best Regards

……………………………………

Joseph Ahn(안연수)

Assistant Software Design Manager

Avnet Electronic Marketing.

Joseph.ahn@avnet.com<mailto:Joseph.ahn@avnet.com>

……………………………………

12th Floor, KBS Media Center, Maebongsan-ro 45 (Sangam-dong),

Mapo-gu, Seoul, 121-915, Korea

Direct:

82-2-6277-6395

Fax:

82-2-761-2133

0 件の賞賛
返信

3,308件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Dear Ahn Joseph,

I think I also handle one of your SR  1-3928133491 regarding to this question.

To switch project from non-floating to floating support, we need replace with the floating support library. See below screenshot:

All the S12Z library file is under this path: C:\Freescale\CW MCU v10.6.4\MCU\S12lisa_Support\s12lisac

2015-07-09_11-40-27.png

  Can this help?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------