S12X CW4.5 function pointers

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S12X CW4.5 function pointers

6,752 次查看
gravity
Contributor I
Hi,
 
S12XDP512, CW 4.5, LARGE memory model
 
I have a function pointer defined as
 
typedef void (*function)(void);
 
I have a void pointer which is holding the function address  0x7DB089'G ( which is actually laid out in memory as B0897D.
 
When I attempt to cast it (or call it) the runtime GLOBAL_TO_LOCAL function is called. The result is
 
0x7DC289 (or  C2897D as laid out in memory). This is incorrect and crashes the code.
 
Any suggestions how I can get around this. I'm guessing that the routine assumes this is a data pointer and not a function pointer?
 
Cheers
 
 
 
标签 (1)
标记 (1)
0 项奖励
回复
7 回复数

3,346 次查看
gravity
Contributor I
Hi,
S12XDP512.
 
The problem was that I was passing the function pointer around using a "void*". I had made this "void*" a "void* far", so it was casting it to global addressing.
 
 
Cheers
 
M
 
 
 
0 项奖励
回复

3,346 次查看
CrasyCat
Specialist III

Hello

 Is the problem fixed now?
 If not, can you send me a code snippet reproducing the trouble.

CrasyCat

0 项奖励
回复

3,346 次查看
CrasyCat
Specialist III

Hello

Which CPU are you currently using (HCS12XDP512, ....)?

From what I can see (from HCS12X reference manual), address 0x7DB089'G is in fact equivalent to address 0xF6B089'L.

All absolute addresses you specify in ANSI C source code are considered as logical (even in large memory model).

So instead of writing

 typedef void (*function)(void);
 function func;


  func = (function) 0x7DB089; 
 
 func();

 You have to write

 typedef void (*function)(void);
 function func;


  func = (function) 0xF6B089; 
 
 func();

CrasyCat

0 项奖励
回复

3,346 次查看
gravity
Contributor I
I think my problem is S12X specific and is to do with translating from a Global address to a local address.
 
The global address is 0x7DB089'G but the local address becomes 0xF6C289'L 
 
 
 
 
0 项奖励
回复

3,346 次查看
gravity
Contributor I
I compiling using large memory model, so I thought everything is a far pointer?
0 项奖励
回复

3,346 次查看
Alban
Senior Contributor II
Sorry, but I can't confirm...
0 项奖励
回复

3,346 次查看
Alban
Senior Contributor II

Hi Gravity,

When you use external address space, you need to use FAR pointers to indicate to the debugger which space you address and avoid address to be truncated or wrong.

See Nabla's post and the code I had on the NE64 with extended bus.

If I understood well what you meant...
Alban.

0 项奖励
回复