S12Z Linker optimization setting
We are trying to implement unit testing for our code .For the unit testing tool to run it create stub functions of all the functions .These stub functions are not referenced in the code .It just needs to be linked in the object file created .
For previous version of codewarrior shown in the screenshot below there was option to keep or remove the unused sections.
Can you please tell how to do in present s12z linker setting .As the linker is removing the unused objects in the object file created .
The present linker optimisation setting is this
Thanks in advance
 
					
				
		
 ZhangJennie
		
			ZhangJennie
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi,
There is no option can avoid all the optimization of compiler.
If a variable or function is never used by program, it may be optimized by compiler. To prevent global variable or function that being optimized, we need take use of “ENTRIES”.
in prm file, there is a section called “ENTRIES”, insert the global variables or functions into this section can avoid they optimized by compiler. For example,
ENTRIES
var1 var2 func1 func2
END
Thus variable var1, var2 and function func1,func2 will not be optimized by compiler.
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------