S08DZ60's Real Time Clock (RTC) interrupt not set in full simulation mode with CW for HC(S)08

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S08DZ60's Real Time Clock (RTC) interrupt not set in full simulation mode with CW for HC(S)08

ソリューションへジャンプ
3,536件の閲覧回数
mayfly
Contributor III
Hi,

I'm developing for a S08DZ60 system.  I am using the RTC to set up a uS/mS clock for non-critical time-based polling. 

Problem:
The RTC interrupt does not get generated in full simulation mode (or the flag doesn't get set?).  It does generate an interrupt in the debugger when in BDM mode (connected to the device).   It also works properly on the device itself when not connected to the debugger.  This would seem to indicate that there's a bug in the debugger. 

I think I saw this in a post before, but try as I might, I couldn't find it again.   Any workarounds?



J2MEJediMaster says: Please remember to add Codewarrior version and MCU type in the subject line.


Message Edited by J2MEJediMaster on 2007-10-04 09:51 AM
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,190件の閲覧回数
CrasyCat
Specialist III
Hello
 
I did try to create a project using Processor Expert with the Project wizard.
I then added a TimerInt Bean to the project and set a period of 1200 ms.
 
I built the project and run it in the simulator and the interrupt gets generated.
The issue might be related to a specific use/configuration of the peripheral.
 
If you feel you have found an issue in simulation however I would recommend you
to submit a service request for that.

Click here to submit a service request.

Make sure to attach a reproducible project and installed product information to the service request.
To generate the required information:
- Start CodeWarrior
- Open the project
- Select "Help" -> "Pack and Go" and follow instructions on the screen.

Attach the generated .zip file to the SR.
 
CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,190件の閲覧回数
CrasyCat
Specialist III
Hello
 
- Which version of CodeWarrior are you using?
  To retrieve that info:
    - Start CodeWarrior
    - Select Help -> About Freescale CodeWarrior
    - Click on "Install Products"
    - CodeWarrior version used is displayed on top in the Installed Products dialog.
 
 
CrasyCat
0 件の賞賛
返信
2,190件の閲覧回数
mayfly
Contributor III
Hi,

The codewarrior version is:
CodeWarrior V6.0 Release, build 7134-30May07

I think the problem is with the Simulator/Debugger:
Version 6.1, build 7134

Thanks

0 件の賞賛
返信
2,191件の閲覧回数
CrasyCat
Specialist III
Hello
 
I did try to create a project using Processor Expert with the Project wizard.
I then added a TimerInt Bean to the project and set a period of 1200 ms.
 
I built the project and run it in the simulator and the interrupt gets generated.
The issue might be related to a specific use/configuration of the peripheral.
 
If you feel you have found an issue in simulation however I would recommend you
to submit a service request for that.

Click here to submit a service request.

Make sure to attach a reproducible project and installed product information to the service request.
To generate the required information:
- Start CodeWarrior
- Open the project
- Select "Help" -> "Pack and Go" and follow instructions on the screen.

Attach the generated .zip file to the SR.
 
CrasyCat
0 件の賞賛
返信