I recall seeing demos showing how easy it is to retarget CW projects from one processor to another -- just a few clicks of the mouse, with minimal editing. However, I can't find instructions for doing this. Maybe I'm looking in the wrong places, or maybe I just imagined this.
I have a project that runs on the MC9S08SH16 but is running out of space, so I want to retarget it to the MC9S08SH32. Any help will be appreciated.
Thanks,
Richly
解決済! 解決策の投稿を見る。
Hello,
You probably linking with a library with no floating point support.
Floating point support is basically done in two places:
- libraries: make sure you have the same library set up as in your previous project. They are in project > Properties > C/C++ Build > Settings > Linker > Input
- For no floating point support, there is a __NO_FLOAT__ define set. Remove it from project > Properties > C/C++ Build > Settings > Compiler > Preprocessor
Hope this helps,
BK
Hello,
you can find the change wizard under the menu Project > Change Device/Connection.
Hope this helps,
BK
Thanks. I had stumbled across that once before and couldn't find it again. If you haven't selected the project, the menu item is greyed out, so I skipped over it many times.
After running the wizard, I got a whole bunch of undefined symbols. Looking at them, I think the problem is that all the floating point routines are missing. Any idea how to convince the newly targeted project to include (32-bit) floating point, which the original target successfully used?
Thanks,
Richly
Hello,
You probably linking with a library with no floating point support.
Floating point support is basically done in two places:
- libraries: make sure you have the same library set up as in your previous project. They are in project > Properties > C/C++ Build > Settings > Linker > Input
- For no floating point support, there is a __NO_FLOAT__ define set. Remove it from project > Properties > C/C++ Build > Settings > Compiler > Preprocessor
Hope this helps,
BK
Many thanks for your excellent information! It solved the floating point problem. I really appreciate your laying out the steps to find the places to change. That made it quite easy.
I should probably two bug reports about retargeting:
(1) the failure to include floating point support
(2) the failure to use the altered values in the linker parameter file (project.prm). I had doubled the stack size and commented out the definition of VECTOR 0, and neither of these made it into the retargeted project.
Thanks again,
Richly
Oops. Found another bug related to retargeting. I am using 32-bit floating point. The retargeting lost two flags: -TD2 and -Fd. I'm not totally sure how to generate both of these, but there are two more things I changed:
(1) project > Properties > C/C++ Build > Settings > HCS08 Compiler > Code Generation
I checked Use IEEE32 for double (default is IEEE64)
(2) project > Properties > C/C++ Build > Settings > HCS08 Compiler > Type Sizes
I selected IEEE32 for double.
These two changes seem to have fixed the problem more completely...but more testing may be necessary!
Cheers,
Richly
Gosh...now another missing piece:
To prevent initialization of RAM at power on reset, the original project had the following definition in the compiler's options:
-D__ONLY_INIT_SP
This is missing in the retargeted project. The only way I could find to generate it was to go to
project > Properties > C/C++ Build > Settings > HCS08 Compiler > Preprocessor
and manually add
__ONLY_INIT_SP
Perhaps the last piece...now the before and after lists of compiler options match each other.
- Richly