Replicated list of variables in Codewarrior 10.6 Debug

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Replicated list of variables in Codewarrior 10.6 Debug

跳至解决方案
1,956 次查看
patrick6772
Contributor I

Hi,

I've been using Codewarrrior 10.4 and recently installed CodeWarrior 10.6.

Everything works fine except that sometimes after I closed and reopened Codewarrior, the list of variables in Debug are replicated multiple times.

Has anyone encountered such a problem or has a solution for it?

Thanks.

标签 (1)
1 解答
1,777 次查看
frankbaird
Contributor III

I had this problem and the fix is to clean your metadata. CW 10 is built upon Eclipse, and the debugger is implemented as an Eclipse plugin. Plugins keep their configuration data in the .metadata folder, and this data can become corrupted. I recently went through the process of doing this. It can be pretty time consuming, but CW works much better now. I followed the instructions here: EclipseZone - Keeping Eclipse running clean ....

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,778 次查看
frankbaird
Contributor III

I had this problem and the fix is to clean your metadata. CW 10 is built upon Eclipse, and the debugger is implemented as an Eclipse plugin. Plugins keep their configuration data in the .metadata folder, and this data can become corrupted. I recently went through the process of doing this. It can be pretty time consuming, but CW works much better now. I followed the instructions here: EclipseZone - Keeping Eclipse running clean ....

0 项奖励
回复
1,777 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Patrick:

Unfortunately this is a known issue in CodeWarrior which has no fix yet. You can find the workaround in the release notes:

pastedImage_0.png

We are sorry for this inconvenience.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------