Removing references to deleted files in project -- old file shows up in Find in Files dialog

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Removing references to deleted files in project -- old file shows up in Find in Files dialog

跳至解决方案
1,593 次查看
tomlogic
Contributor III

I'm going a little crazy trying to figure this one out.  I used to have a header called "endian.h" in my project.  I renamed it, and now it does not appear in the "Files" or "Link Order" tab of the project.

 

But, whenever I do a Find in Files, it shows up in the list of files for Project headers.  If I search all of the files in the project for "endian.h", it only shows up in comments of other files.  If I double-click on the entry in the Find in Files dialog, CW complains that it can't find the file (which is expected, since I deleted it) and it allows me to remove it from the list.

 

But as soon as I do another Find in Files, it's right back in there.

 

What do I need to do for CW to forget that the file ever existed?

 

-Tom

(CodeWarrior 5.9.0 on S08 processor)

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,142 次查看
kef
Specialist I

I would try deleting projectname_Data folder. You need to close project first.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,143 次查看
kef
Specialist I

I would try deleting projectname_Data folder. You need to close project first.

0 项奖励
回复
1,142 次查看
tomlogic
Contributor III

Brilliant.  That did the trick.  Thanks!

0 项奖励
回复