Reg: DSC flash programmer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reg: DSC flash programmer

ソリューションへジャンプ
1,969件の閲覧回数
dharanidevimani
Contributor I

Is the flash programmer of DSC 56800E is available for Windows 64-bit version?. I have FLSHPROGRAMMER_V1.2_WIN32 file, We purchased a new laptop with 64-bit version. So its not getting supported. Please help me on this

ラベル(1)
0 件の賞賛
返信
1 解決策
1,836件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

Refer to Is the flash programmer of DSC 56800E is available for Windows 64-bit version?. I have FLSHPROGRAMME...


Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,836件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

Refer to Is the flash programmer of DSC 56800E is available for Windows 64-bit version?. I have FLSHPROGRAMME...


Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信