RTI interrupt with external clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RTI interrupt with external clock

ソリューションへジャンプ
5,974件の閲覧回数
Diana
Contributor I

Hello,

 

I need to create a time interruption to send some data, and I have choose RTI interrupt, but it don't run.

 

The interruptions is:

 

 /////////////////////////////

__interrupt 25 void Vrti_isr(void)

{

SRTISC_RTIACK=1;

tiempo=1;     // when this variables is 1 I send the dates.

} 

//////////////////// 

 

In the main funcion I inicialize de interrupt with:

 

  SRTISC=0x77; // I use external clock of 62,5kHz because we are on run mode

  EnableInterrupts;  

 

 What is wrong? 

Is there any easy way to make a break in time? 
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
4,318件の閲覧回数
peg
Senior Contributor IV

Hi Diana,

 

It seems setup correctly to me!

 

A couple of things though:

I thought the SARD's MPU used the clock output from the radio device for its clock (16MHz?)

 

If you are only going to set a flag in the ISR for later use you may as well not enable interrupts and simply test the RTIF bit in SRTISC. (still need to ACK it)

 

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
4,318件の閲覧回数
peg
Senior Contributor IV

Hello Diana,

 

You need to tell us what part you are using.

With some devices the RTI does not function in all clock modes.

 

0 件の賞賛
返信
4,318件の閲覧回数
Diana
Contributor I

Hello,

I am using 13192sard, with MC9S08GT60 44pins microcontroller. The frecuency of its external clock is 62.5kHz. I need send information to the PC every minute and had thought with a interrupt RTI.

 

 

 

0 件の賞賛
返信
4,319件の閲覧回数
peg
Senior Contributor IV

Hi Diana,

 

It seems setup correctly to me!

 

A couple of things though:

I thought the SARD's MPU used the clock output from the radio device for its clock (16MHz?)

 

If you are only going to set a flag in the ISR for later use you may as well not enable interrupts and simply test the RTIF bit in SRTISC. (still need to ACK it)

 

0 件の賞賛
返信
4,318件の閲覧回数
Diana
Contributor I

Hi Pej,

 

I had found this frecuency in the next file.

 

MC13192_EVBRM.pdf

Message Edited by t.dowe on 2009-10-22 09:14 AM
0 件の賞賛
返信
4,318件の閲覧回数
peg
Senior Contributor IV

Hello Diana,

 

You mentioned SARD before now you are talking EVB!

It does say 62.5kHz here but the output of the radio is programmable so you would need to check. You could also test it at TP6.

It should still work though.