Programming process with Multilink Universal?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programming process with Multilink Universal?

1,504件の閲覧回数
luiscahuich
Contributor II

Good Evening

Could someone tell me wich is the process to program a target, for example a JM60 with the Multilink Universal?

I am working with Codewarrior V10.6

As far as i understand I can program the device and I can debug the device.

How can i Do both of them? Which are the steps to follow?

Thank you so much in advance?

ラベル(1)
0 件の賞賛
返信
1 返信

1,457件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Luis

To program and debug the device, please right-click on your project name, and select "Debug As -> Debug Configuration".

MENU.png

Then choose the correct connection type, and click on Debug button. The debugger starts programming the MCU with your firmware, after programming, user can start the debugging in IDE.

debug.png

For how to use the debugger, please refer to  <Chapter 4 Working with Debugger> in Targeting Manual:

http://cache.nxp.com/files/soft_dev_tools/doc/user_guide/CWMCUDBGUG.pdf  

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信