Programming from DOS shell MCU MM9Z1J638 problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Programming from DOS shell MCU MM9Z1J638 problem

2,516 Views
evm11
Contributor I

Hello

I try to programming MM9Z1J638 from DOS shell. I use CW 11.1 and programmer Multilink Universal FX.

I made tcl file for that:

fl::disconnect
fl::target -lc "LC for Simple Flash"
fl::target -b 0x1000 0x2000
fl::target -v off -l off
cmdwin::fl::device -d "MM9Z1J638_FLASH" -o "128Kx32x1" -a 0xfe0000 0xffffff
cmdwin::fl::protect all off
cmdwin::fl::device -d "MM9Z1J638_EEPROM" -o "4Kx32x1" -a 0x100000 0x100fff
cmdwin::fl::protect all off
cmdwin::fl::device -d "MM9Z1J638_FLASH" -o "128Kx32x1" -a 0xfe0000 0xffffff
cmdwin::fl::image -f "C:\\LEM\\IN200\\BATS2_prj\\G16001C-Volvo-embBoot.elf" -t "Auto Detect" -re on -r 0xfe0000 0xffffff -oe off
cmdwin::fl::erase image
cmdwin::fl::write
cmdwin::fl::device -d "MM9Z1J638_EEPROM" -o "4Kx32x1" -a 0x100000 0x100fff
cmdwin::fl::image -f "C:\\LEM\\IN200\\BATS2_prj\\G16001C-Volvo-embBoot.elf" -t "Auto Detect" -re on -r 0x100000 0x100fff -oe off
cmdwin::fl::erase image
cmdwin::fl::write
fl::disconnect
quitIDE
exit

But after run this script I receive error:

CodeWarrior Debugger Shell v1.0
%>source C:\LEM\IN200\BATS2_prj\bats2\b_t.tcl
cmdwin::fl::disconnect
cmdwin::fl::target -lc LC for Simple Flash
cmdwin::fl::target -b 0x1000 0x2000
cmdwin::fl::target -v off -l off
cmdwin::fl::device -d MM9Z1J638_FLASH -o 128Kx32x1 -a 0xfe0000 0xffffff
cmdwin::fl::protect all off
Flash Programmer internal error: connection list is empty
Beginning Operation ...
-------------------------
Error: Operation failed. GetFlashDriverFile: Algorithm file C:\Freescale\CW MCU
v11.1\MCU\bin\Plugins\Support\Flash_Programme
r\ is not an elf file. Flash drivers must be elf images.
Error: Couldn't open flash driver file.
Error: Operation failed.GetFlashDriverFile: Algorithm file C:\Freescale\CW MCU
v11.1\MCU\bin\Plugins\Support\Flash_Programmer\ is
not an elf file. Flash drivers must be elf images.

What I can do with that or where I mistake?

0 Kudos
Reply
3 Replies

2,500 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Jevgeni,

I have contacted an application engineer with your description of the issue. He need some additional data. Please provide them. Please see the description.

DESCRIPTION

Could you show me the content of b_t.tcl so I can take a look at whether the tickle script has the right commands?

With Best Regards,

Jozef

0 Kudos
Reply

2,496 Views
evm11
Contributor I

Hello Jozef

Thanks for you replay.

The script file b_t.tcl is attached.

BR, Jevgeni

0 Kudos
Reply

2,492 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Jevgeni,

could you please send the content of the b_t.tcl file in .pdf or in any other text document? I cannot open it on my computer and I can send the application engineer in a community text only. 

With Best Regards,

Jozef

0 Kudos
Reply