Programming HCS08 on Raspberry Pi

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Programming HCS08 on Raspberry Pi

2,758 Views
edasanli
Contributor I

I need to programming MC9S08PA4 on Raspberry Pi. I tried to install Code Warrior on RPi, but RPi is based on ARM so it could not install. I don't need to developing, I have a s19 file, just need to programming my microprocessor.

Is there someone have a solution about that? 

Have a nice day. 

-Eda 

#mc9s08pa4‌raspberry pi‌

Labels (1)
0 Kudos
Reply
2 Replies

2,702 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

In order to program the S08 you will need an OSBDM, those are available on several evaluation boards or in programmers like the Universal multilink from P&E.

or you can create your own OSBDM, please check 

PEmicro | Experts in Embedded tools for Flash Programming and Development 

I hope this will help you

Regards

Vicente 

0 Kudos
Reply

2,702 Views
edasanli
Contributor I

I have S08PT60-EVK and PE Micro Multilink. But I need an application for programming, which can be installed on Raspberry Pi.

0 Kudos
Reply